SimLoadRecipeFunctionAttributes Class¶
-
class
NXOpen.CAE.
SimLoadRecipeFunctionAttributes
¶ Bases:
NXOpen.TaggedObject
This is the class handling the default attributes of a source used by a load recipe. This is used by data sources which cannot derive these attributes from the file itself (like UNV, OP2, …). They specify the default attributes of all functions in the file. Whenever this object is modified, a call to UPDATE_do_update is needed in order to propagate the changes to the LoadRecipe.
Use CAE.SimLoadRecipeSource.GetFunctionAttributes
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AcousticalWeighting | Returns or sets the default acoustical weighting of the functions in the file |
AmplitudeCorrectionFactor | Returns or sets the default amplitude correction factor of the functions in the file |
CorrectionMode | Returns or sets the default correction mode of the functions in the file |
EnergyCorrectionFactor | Returns or sets the default energy correction factor of the functions in the file |
SpectrumScaling | Returns or sets the default spectrum scaling of the functions in the file |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
SimLoadRecipeFunctionAttributesAcousticalWeightings Enumeration | This enum defines the acoustical weightings |
SimLoadRecipeFunctionAttributesCorrectionModes Enumeration | This enum defines the correction modes |
SimLoadRecipeFunctionAttributesScalingType Enumeration | This enum defines the spectrum scaling |
Property Detail¶
AcousticalWeighting¶
-
SimLoadRecipeFunctionAttributes.
AcousticalWeighting
¶ Returns or sets the default acoustical weighting of the functions in the file
-------------------------------------
Getter Method
Signature
AcousticalWeighting
Returns: Return type: NXOpen.CAE.SimLoadRecipeFunctionAttributesAcousticalWeightings
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AcousticalWeighting
Parameters: weighting ( NXOpen.CAE.SimLoadRecipeFunctionAttributesAcousticalWeightings
) –New in version NX12.0.0.
License requirements: None.
AmplitudeCorrectionFactor¶
-
SimLoadRecipeFunctionAttributes.
AmplitudeCorrectionFactor
¶ Returns or sets the default amplitude correction factor of the functions in the file
-------------------------------------
Getter Method
Signature
AmplitudeCorrectionFactor
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AmplitudeCorrectionFactor
Parameters: correctionFactor (float) – New in version NX12.0.0.
License requirements: None.
CorrectionMode¶
-
SimLoadRecipeFunctionAttributes.
CorrectionMode
¶ Returns or sets the default correction mode of the functions in the file
-------------------------------------
Getter Method
Signature
CorrectionMode
Returns: Return type: NXOpen.CAE.SimLoadRecipeFunctionAttributesCorrectionModes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CorrectionMode
Parameters: correctionMode ( NXOpen.CAE.SimLoadRecipeFunctionAttributesCorrectionModes
) –New in version NX12.0.0.
License requirements: None.
EnergyCorrectionFactor¶
-
SimLoadRecipeFunctionAttributes.
EnergyCorrectionFactor
¶ Returns or sets the default energy correction factor of the functions in the file
-------------------------------------
Getter Method
Signature
EnergyCorrectionFactor
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnergyCorrectionFactor
Parameters: correctionFactor (float) – New in version NX12.0.0.
License requirements: None.
SpectrumScaling¶
-
SimLoadRecipeFunctionAttributes.
SpectrumScaling
¶ Returns or sets the default spectrum scaling of the functions in the file
-------------------------------------
Getter Method
Signature
SpectrumScaling
Returns: Return type: NXOpen.CAE.SimLoadRecipeFunctionAttributesScalingType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpectrumScaling
Parameters: spectrumScaling ( NXOpen.CAE.SimLoadRecipeFunctionAttributesScalingType
) –New in version NX12.0.0.
License requirements: None.