VelocityImpactExcitationBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
VelocityImpactExcitationBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.ExcitationBuilder
Represents a
NXOpen.CAE.ResponseSimulation.VelocityImpactExcitationBuilder
To create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.ExcitationCollection.CreateVelocityImpactExcitationBuilder()
Default values.
Property Value ImpactDirection.DirectionOption NodalComponent ImpactDirection.NodalComponent Dof1 ImpactMethod ConstantVelocity ImpactParameters.DropHeight.Value 1.0 (millimeters part), 1.0 (inches part) ImpactParameters.PulseDuration.Value 1.0 (millimeters part), 1.0 (inches part) ImpactParameters.StartPosition AtDrop ImpactParameters.TimeStep.Value 1.0 (millimeters part), 1.0 (inches part) ImpactParameters.Velocity.Value 1.0 (millimeters part), 1.0 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DynamicEvent | Returns the parent dynamic event object |
ExcitationLocationDefinition | Returns the excitation location definition |
ImpactDirection | Returns the impact direction setting |
ImpactMethod | Returns or sets the impact method |
ImpactParameters | Returns the impact parameters setting |
ObjectLabel | Returns the object label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
VelocityImpactExcitationBuilderImpactMethodType Enumeration | the impact definiton methods |
Property Detail¶
ImpactDirection¶
-
VelocityImpactExcitationBuilder.
ImpactDirection
¶ Returns the impact direction setting
-------------------------------------
Getter Method
Signature
ImpactDirection
Returns: Return type: NXOpen.CAE.ResponseSimulation.VelocityImpactDirection
New in version NX6.0.0.
License requirements: None.
ImpactMethod¶
-
VelocityImpactExcitationBuilder.
ImpactMethod
¶ Returns or sets the impact method
-------------------------------------
Getter Method
Signature
ImpactMethod
Returns: Return type: NXOpen.CAE.ResponseSimulation.VelocityImpactExcitationBuilderImpactMethodType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImpactMethod
Parameters: impactMethod ( NXOpen.CAE.ResponseSimulation.VelocityImpactExcitationBuilderImpactMethodType
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ImpactParameters¶
-
VelocityImpactExcitationBuilder.
ImpactParameters
¶ Returns the impact parameters setting
-------------------------------------
Getter Method
Signature
ImpactParameters
Returns: Return type: NXOpen.CAE.ResponseSimulation.VelocityImpactParameters
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
VelocityImpactExcitationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.