VelocityImpactExcitationBuilderImpactMethodType Enumeration¶
NXOpen.CAE.ResponseSimulation.VelocityImpactExcitationBuilder.ImpactMethodType is an alias for NXOpen.CAE.ResponseSimulation.VelocityImpactExcitationBuilderImpactMethodType
-
class
NXOpen.CAE.ResponseSimulation.
VelocityImpactExcitationBuilderImpactMethodType
¶ Bases:
object
the impact definiton methods
Enum Members
Enum Member Enum Member Description ConstantVelocity the users will only be able to specify the velocity for the impact DropImpact the users will be able to specify the drop height or the desired velocity at the impact -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-