TransmissibilityEvaluationSettingBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
TransmissibilityEvaluationSettingBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.ModalResultsEvaluationSettingBuilder
This is a manager to the
NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSetting
class.Object of type
NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSetting
can be created and edited only through this classTo create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.EvaluationSettingManager.CreateTransmissibilityEvaluationSettingBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DataLocation | Returns the frequency setting |
EvaluationProperty | Returns the frequency setting |
InputDirection | Returns or sets the source direction data component |
InputMotionType | Returns or sets the input motion type |
InputNode | Returns or sets the source node. |
ObservationNode | Returns or sets the observation nodes. |
OutputRequest | Returns or sets the destination direction data component |
OutputSettings | Returns the output setting. |
ResultType | Returns or sets the result type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputElements | Returns destination nodes. |
GetOutputNodes | Returns destination nodes. |
SetOutputElements | Sets destination nodes |
SetOutputNodes | Sets destination nodes |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TransmissibilityEvaluationSettingBuilderMotionType Enumeration | This enum defines input motion type |
Property Detail¶
InputMotionType¶
-
TransmissibilityEvaluationSettingBuilder.
InputMotionType
¶ Returns or sets the input motion type
-------------------------------------
Getter Method
Signature
InputMotionType
Returns: Return type: NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSettingBuilderMotionType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
InputMotionType
Parameters: motionType ( NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSettingBuilderMotionType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
Validate¶
-
TransmissibilityEvaluationSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.