TransmissibilityEvaluationSettingBuilderMotionType Enumeration

NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSettingBuilder.MotionType is an alias for NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSettingBuilderMotionType

class NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSettingBuilderMotionType

Bases: object

This enum defines input motion type

Enum Members

Enum Member Enum Member Description
Displacement
Velocity
Acceleration
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.