TranslationalNodalFunctionExcitationBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
TranslationalNodalFunctionExcitationBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.NodalFunctionExcitationBuilder
Represents the manager to
NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitation
.The objects of
NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitation
can be created or edited on through this class To create a new instance of this class, useNXOpen.CAE.ResponseSimulation.ExcitationCollection.CreateTranslationalNodalFunctionExcitationBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DynamicEvent | Returns the parent dynamic event object |
EnableUserDefinedDirection | Returns or sets the excitation function definition method |
EnableUserDefinedRotation | Returns or sets the excitation function definition method |
ExcitationLocationDefinition | Returns the excitation location definition |
FunctionComponentX | Returns the function component of X direction |
FunctionComponentY | Returns the function component of Y direction |
FunctionComponentZ | Returns the function component of Z direction |
ObjectLabel | Returns the object label |
RotationAxis | Returns or sets the rotation axis |
Tag | Returns the Tag for this object. |
UserDefinedDirection | Returns or sets the magnitude direction |
UserDefinedFunction | Returns the magnitude function |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TranslationalNodalFunctionExcitationBuilderRotationAxisType Enumeration | Represents the rotation axis type. |
Property Detail¶
EnableUserDefinedDirection¶
-
TranslationalNodalFunctionExcitationBuilder.
EnableUserDefinedDirection
¶ Returns or sets the excitation function definition method
-------------------------------------
Getter Method
Signature
EnableUserDefinedDirection
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
EnableUserDefinedDirection
Parameters: enableUserDefinedDirection (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EnableUserDefinedRotation¶
-
TranslationalNodalFunctionExcitationBuilder.
EnableUserDefinedRotation
¶ Returns or sets the excitation function definition method
-------------------------------------
Getter Method
Signature
EnableUserDefinedRotation
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
EnableUserDefinedRotation
Parameters: enableUserDefinedRotation (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FunctionComponentX¶
-
TranslationalNodalFunctionExcitationBuilder.
FunctionComponentX
¶ Returns the function component of X direction
-------------------------------------
Getter Method
Signature
FunctionComponentX
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FunctionComponentY¶
-
TranslationalNodalFunctionExcitationBuilder.
FunctionComponentY
¶ Returns the function component of Y direction
-------------------------------------
Getter Method
Signature
FunctionComponentY
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FunctionComponentZ¶
-
TranslationalNodalFunctionExcitationBuilder.
FunctionComponentZ
¶ Returns the function component of Z direction
-------------------------------------
Getter Method
Signature
FunctionComponentZ
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
RotationAxis¶
-
TranslationalNodalFunctionExcitationBuilder.
RotationAxis
¶ Returns or sets the rotation axis
-------------------------------------
Getter Method
Signature
RotationAxis
Returns: Return type: NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitationBuilderRotationAxisType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
RotationAxis
Parameters: rotationAxis ( NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitationBuilderRotationAxisType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
UserDefinedDirection¶
-
TranslationalNodalFunctionExcitationBuilder.
UserDefinedDirection
¶ Returns or sets the magnitude direction
-------------------------------------
Getter Method
Signature
UserDefinedDirection
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
UserDefinedDirection
Parameters: magnitudeDirection ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
UserDefinedFunction¶
-
TranslationalNodalFunctionExcitationBuilder.
UserDefinedFunction
¶ Returns the magnitude function
-------------------------------------
Getter Method
Signature
UserDefinedFunction
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
Validate¶
-
TranslationalNodalFunctionExcitationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.