FunctionComponentData Class¶
-
class
NXOpen.CAE.ResponseSimulation.
FunctionComponentData
¶ Bases:
NXOpen.TaggedObject
Represents a function component setting of
NXOpen.CAE.ResponseSimulation.NodalFunctionExcitation
on one directionNew in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Enable | Returns or sets the option to enable the function component to be used while evaluating |
Function | Returns or sets the function to be applied |
PhaseAngle | Returns or sets the phase angle. |
ScalarFactor | Returns or sets the scalar factor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetComponentType | Returns the component type |
Property Detail¶
Enable¶
-
FunctionComponentData.
Enable
¶ Returns or sets the option to enable the function component to be used while evaluating
-------------------------------------
Getter Method
Signature
Enable
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
Enable
Parameters: enableOption (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Function¶
-
FunctionComponentData.
Function
¶ Returns or sets the function to be applied
-------------------------------------
Getter Method
Signature
Function
Returns: Return type: NXOpen.CAE.Function
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
Function
Parameters: excitationFunction ( NXOpen.CAE.Function
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
PhaseAngle¶
-
FunctionComponentData.
PhaseAngle
¶ Returns or sets the phase angle.
Only available when the onwer event is
NXOpen.CAE.ResponseSimulation.RSEventType.Transient
-------------------------------------
Getter Method
Signature
PhaseAngle
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
PhaseAngle
Parameters: phaseAngle (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ScalarFactor¶
-
FunctionComponentData.
ScalarFactor
¶ Returns or sets the scalar factor
-------------------------------------
Getter Method
Signature
ScalarFactor
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ScalarFactor
Parameters: scalarFactor (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetComponentType¶
-
FunctionComponentData.
GetComponentType
¶ Returns the component type
Signature
GetComponentType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ExcitationComponent
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)