ExcitationComponent Enumeration

NXOpen.CAE.ResponseSimulation.Excitation.Component is an alias for NXOpen.CAE.ResponseSimulation.ExcitationComponent

class NXOpen.CAE.ResponseSimulation.ExcitationComponent

Bases: object

Represents the component type.

Enum Members

Enum Member Enum Member Description
DistributedLoad
X
Y
Z
Rx
Ry
Rz
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.