PrlResultsEvaluationSettingBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
PrlResultsEvaluationSettingBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.DynamicResultEvaluationSettingBuilder
Represents the abstract builder class of evaluation setting for peak value, RMS results and LCR results.
This is an abstract class, and cannot be created.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CoordinateSystem | Returns or sets the coordinate system. |
ObservationNode | Returns or sets the relative node. |
Relative | Returns or sets the option of using the observation node in evaluation |
ResultType | Returns or sets the result type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDataComponents | Returns the direction data components. |
GetDescriptionString | Returns the description. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputElements | Returns the destination elements. |
GetOutputNodes | Returns the destination nodes. |
SetDataComponents | Sets the direction data components. |
SetDescriptionString | Sets the description |
SetOutputElements | Sets the destination elements |
SetOutputNodes | Sets the destination nodes |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CoordinateSystem¶
-
PrlResultsEvaluationSettingBuilder.
CoordinateSystem
¶ Returns or sets the coordinate system.
Only available when the result type is
NXOpen.CAE.ResponseSimulation.EvaluationResultType.Stress
,NXOpen.CAE.ResponseSimulation.EvaluationResultType.ShellResultant
-------------------------------------
Getter Method
Signature
CoordinateSystem
Returns: Return type: NXOpen.CAE.ResponseSimulation.CoordinateSystem
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
CoordinateSystem
Parameters: coordinateSystem ( NXOpen.CAE.ResponseSimulation.CoordinateSystem
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ObservationNode¶
-
PrlResultsEvaluationSettingBuilder.
ObservationNode
¶ Returns or sets the relative node.
Only available when result type is
NXOpen.CAE.ResponseSimulation.EvaluationResultType.Displacement
,NXOpen.CAE.ResponseSimulation.EvaluationResultType.Acceleration
,NXOpen.CAE.ResponseSimulation.EvaluationResultType.ElementForce
-------------------------------------
Getter Method
Signature
ObservationNode
Returns: Return type: NXOpen.CAE.FENode
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ObservationNode
Parameters: relativeNode ( NXOpen.CAE.FENode
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Relative¶
-
PrlResultsEvaluationSettingBuilder.
Relative
¶ Returns or sets the option of using the observation node in evaluation
-------------------------------------
Getter Method
Signature
Relative
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
Relative
Parameters: relative (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ResultType¶
-
PrlResultsEvaluationSettingBuilder.
ResultType
¶ Returns or sets the result type
-------------------------------------
Getter Method
Signature
ResultType
Returns: Return type: NXOpen.CAE.ResponseSimulation.EvaluationResultType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ResultType
Parameters: resultType ( NXOpen.CAE.ResponseSimulation.EvaluationResultType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetDataComponents¶
-
PrlResultsEvaluationSettingBuilder.
GetDataComponents
¶ Returns the direction data components.
The condidate choices will be changed according to
NXOpen.CAE.ResponseSimulation.EvaluationResultType
settingSignature
GetDataComponents()
Returns: Return type: list of NXOpen.CAE.ResponseSimulation.DirectionDataComponent
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetOutputElements¶
-
PrlResultsEvaluationSettingBuilder.
GetOutputElements
¶ Returns the destination elements.
Only available when the result type is
NXOpen.CAE.ResponseSimulation.EvaluationResultType.Stress
,NXOpen.CAE.ResponseSimulation.EvaluationResultType.ShellResultant
Signature
GetOutputElements()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetOutputNodes¶
-
PrlResultsEvaluationSettingBuilder.
GetOutputNodes
¶ Returns the destination nodes.
Only available when result type is
NXOpen.CAE.ResponseSimulation.EvaluationResultType.Displacement
,NXOpen.CAE.ResponseSimulation.EvaluationResultType.Acceleration
,NXOpen.CAE.ResponseSimulation.EvaluationResultType.ElementForce
Signature
GetOutputNodes()
Returns: Return type: list of NXOpen.CAE.FENode
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetDataComponents¶
-
PrlResultsEvaluationSettingBuilder.
SetDataComponents
¶ Sets the direction data components.
The condidate choices will be changed according to
NXOpen.CAE.ResponseSimulation.EvaluationResultType
settingSignature
SetDataComponents(dataComponent)
Parameters: dataComponent (list of NXOpen.CAE.ResponseSimulation.DirectionDataComponent
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetOutputElements¶
-
PrlResultsEvaluationSettingBuilder.
SetOutputElements
¶ Sets the destination elements
Signature
SetOutputElements(destinationElements)
Parameters: destinationElements (list of NXOpen.CAE.FEElement
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetOutputNodes¶
-
PrlResultsEvaluationSettingBuilder.
SetOutputNodes
¶ Sets the destination nodes
Signature
SetOutputNodes(destinationNodes)
Parameters: destinationNodes (list of NXOpen.CAE.FENode
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Validate¶
-
PrlResultsEvaluationSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.