DirectionDataComponent Enumeration¶
-
class
NXOpen.CAE.ResponseSimulation.
DirectionDataComponent
¶ Bases:
object
Specifies the direction data components Enum Members
Enum Member Enum Member Description X Y Z Rx Ry Rz Xx Yy Zz Xy Xz Yz Ax Sy Sz Tx Byy Bz Fxx Fyy Fzz Fxy Mx My Mz Mxy Mxz Myz Vx Vy TranslationalMagnitude Vonmises MaxPrincipal MinPrincipal MaxShear AllNormals AllTranslational AllForces AllDirections AllDataComponents All AllXyPlane Leg1 Leg2 Leg3 AllLegs -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-