FrequencyDefinition Class¶
-
class
NXOpen.CAE.ResponseSimulation.
FrequencyDefinition
¶ Bases:
NXOpen.TaggedObject
Represents the frequency setting to perform FRF evaluation
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ContributorNumber | Returns or sets the number of contributors. |
EndValue | Returns or sets the end value of frequency range. |
EvaluationType | Returns or sets the method to define frequency |
GenerateMaximumContributors | Returns or sets the option for generating maximum contributors or not. |
InterpolationMethodOption | Returns or sets the interpolation method. |
NormalizeResults | Returns or sets the option to normalize results. |
SpectralLine | Returns or sets the additional spectral lines. |
StartValue | Returns or sets the start value of frequency range. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetFrequencies | Returns frequency values to perform FRF evaluation. |
SetFrequencies | Sets the frequency values to perform FRF evaluation. |
Enumerations¶
FrequencyDefinitionDefinition Enumeration | Specifies the method to define frequency |
FrequencyDefinitionInterpolationMethod Enumeration | Specifies the method for interpolation |
Property Detail¶
ContributorNumber¶
-
FrequencyDefinition.
ContributorNumber
¶ Returns or sets the number of contributors.
Only available when maximu contributors will be generated
-------------------------------------
Getter Method
Signature
ContributorNumber
Returns: Return type: int New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ContributorNumber
Parameters: contributorNumber (int) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EndValue¶
-
FrequencyDefinition.
EndValue
¶ Returns or sets the end value of frequency range.
Only available when the frequency is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
EndValue
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
EndValue
Parameters: endValue (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EvaluationType¶
-
FrequencyDefinition.
EvaluationType
¶ Returns or sets the method to define frequency
-------------------------------------
Getter Method
Signature
EvaluationType
Returns: Return type: NXOpen.CAE.ResponseSimulation.FrequencyDefinitionDefinition
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
EvaluationType
Parameters: type ( NXOpen.CAE.ResponseSimulation.FrequencyDefinitionDefinition
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GenerateMaximumContributors¶
-
FrequencyDefinition.
GenerateMaximumContributors
¶ Returns or sets the option for generating maximum contributors or not.
Only available when frequency definition metod is
CAE.ResponseSimulation.FrequencyDefinitionDefinition.ModalContribution
-------------------------------------
Getter Method
Signature
GenerateMaximumContributors
Returns: Return type: bool New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
GenerateMaximumContributors
Parameters: generateMaximumContributors (bool) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
InterpolationMethodOption¶
-
FrequencyDefinition.
InterpolationMethodOption
¶ Returns or sets the interpolation method.
Only available when the frequency is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
InterpolationMethodOption
Returns: Return type: NXOpen.CAE.ResponseSimulation.FrequencyDefinitionInterpolationMethod
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
InterpolationMethodOption
Parameters: interpolationMethod ( NXOpen.CAE.ResponseSimulation.FrequencyDefinitionInterpolationMethod
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
NormalizeResults¶
-
FrequencyDefinition.
NormalizeResults
¶ Returns or sets the option to normalize results.
Only available when maximu contributors will be generated
-------------------------------------
Getter Method
Signature
NormalizeResults
Returns: Return type: bool New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
NormalizeResults
Parameters: normalizeResults (bool) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SpectralLine¶
-
FrequencyDefinition.
SpectralLine
¶ Returns or sets the additional spectral lines.
Only available when frequency is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
SpectralLine
Returns: Return type: int New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
SpectralLine
Parameters: spectralLines (int) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
StartValue¶
-
FrequencyDefinition.
StartValue
¶ Returns or sets the start value of frequency range.
Only available when the frequency is defined by
CAE.ResponseSimulation.FrequencyDefinitionDefinition.Range
-------------------------------------
Getter Method
Signature
StartValue
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
StartValue
Parameters: startValue (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetFrequencies¶
-
FrequencyDefinition.
GetFrequencies
¶ Returns frequency values to perform FRF evaluation.
Only available when the frequency definition method is
CAE.ResponseSimulation.FrequencyDefinitionDefinition.ModalContribution
Signature
GetFrequencies()
Returns: Return type: list of float New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetFrequencies¶
-
FrequencyDefinition.
SetFrequencies
¶ Sets the frequency values to perform FRF evaluation.
Only available when the frequency definition method is
CAE.ResponseSimulation.FrequencyDefinitionDefinition.ModalContribution
Signature
SetFrequencies(frequencies)
Parameters: frequencies (list of float) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)