FrequencyDefinitionDefinition Enumeration

NXOpen.CAE.ResponseSimulation.FrequencyDefinition.Definition is an alias for NXOpen.CAE.ResponseSimulation.FrequencyDefinitionDefinition

class NXOpen.CAE.ResponseSimulation.FrequencyDefinitionDefinition

Bases: object

Specifies the method to define frequency

Enum Members

Enum Member Enum Member Description
Range
ModalContribution
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.