PreTestSensorConfigBuilder Class¶
-
class
NXOpen.CAE.
PreTestSensorConfigBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.PreTestSensorConfig
builderTo create a new instance of this class, use
NXOpen.CAE.PreTestSolutionCollection.CreateSensorConfigBuilder()
Default values.
Property Value AlgorithmChoice MinMac NumTriaxialSensors 0 NumUniaxialSensors 10 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AlgorithmChoice | Returns or sets the sensor selection algorithm |
Name | Returns or sets the name |
NumTriaxialSensors | Returns or sets the number of triaxial sensors to select |
NumUniaxialSensors | Returns or sets the number of uniaxial sensors to select |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreTestSensorConfigBuilderAlgorithmChoiceType Enumeration | Selected algorithm for the sensor selection |
Property Detail¶
AlgorithmChoice¶
-
PreTestSensorConfigBuilder.
AlgorithmChoice
¶ Returns or sets the sensor selection algorithm
-------------------------------------
Getter Method
Signature
AlgorithmChoice
Returns: Return type: NXOpen.CAE.PreTestSensorConfigBuilderAlgorithmChoiceType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlgorithmChoice
Parameters: algorithmChoice ( NXOpen.CAE.PreTestSensorConfigBuilderAlgorithmChoiceType
) –New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Name¶
-
PreTestSensorConfigBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
NumTriaxialSensors¶
-
PreTestSensorConfigBuilder.
NumTriaxialSensors
¶ Returns or sets the number of triaxial sensors to select
-------------------------------------
Getter Method
Signature
NumTriaxialSensors
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumTriaxialSensors
Parameters: numTriaxialSensors (int) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
NumUniaxialSensors¶
-
PreTestSensorConfigBuilder.
NumUniaxialSensors
¶ Returns or sets the number of uniaxial sensors to select
-------------------------------------
Getter Method
Signature
NumUniaxialSensors
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumUniaxialSensors
Parameters: numUniaxialSensors (int) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
Validate¶
-
PreTestSensorConfigBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.