PreTestSensorConfigBuilderAlgorithmChoiceType Enumeration

NXOpen.CAE.PreTestSensorConfigBuilder.AlgorithmChoiceType is an alias for NXOpen.CAE.PreTestSensorConfigBuilderAlgorithmChoiceType

class NXOpen.CAE.PreTestSensorConfigBuilderAlgorithmChoiceType

Bases: object

Selected algorithm for the sensor selection

Enum Members

Enum Member Enum Member Description
MinMac
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.