NumberFormat Class¶
-
class
NXOpen.CAE.
NumberFormat
¶ Bases:
NXOpen.TaggedObject
Represents the settings of format number value
New in version NX11.0.2.
Properties¶
Property | Description |
---|---|
DecimalPlaces | Returns or sets the decimal places. |
Format | Returns or sets the format option |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
NumberFormatFormatOption Enumeration | Represents the format option |
Property Detail¶
DecimalPlaces¶
-
NumberFormat.
DecimalPlaces
¶ Returns or sets the decimal places.
The value should be between 0 and 9.
-------------------------------------
Getter Method
Signature
DecimalPlaces
Returns: Return type: int New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
DecimalPlaces
Parameters: decimalPlaces (int) – New in version NX11.0.2.
License requirements: None.
Format¶
-
NumberFormat.
Format
¶ Returns or sets the format option
-------------------------------------
Getter Method
Signature
Format
Returns: Return type: NXOpen.CAE.NumberFormatFormatOption
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Format
Parameters: format ( NXOpen.CAE.NumberFormatFormatOption
) –New in version NX11.0.2.
License requirements: None.