NumberFormatFormatOption Enumeration¶
NXOpen.CAE.NumberFormat.FormatOption is an alias for NXOpen.CAE.NumberFormatFormatOption
-
class
NXOpen.CAE.
NumberFormatFormatOption
¶ Bases:
object
Represents the format option
Enum Members
Enum Member Enum Member Description Automatic The program will determine the format internally Fixed Format the number in fixed decimals Scientific Format the number in scientific -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-