NodeReflectBuilder Class¶
-
class
NXOpen.CAE.
NodeReflectBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodeReflectBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodeReflectBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CopyOption | Returns or sets the copy option |
Increment | Returns or sets the increment |
Label | Returns or sets the label |
LabelOption | Returns or sets the label option |
Node | Returns the node |
Offset | Returns or sets the offset |
Plane | Returns or sets the plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NodeReflectBuilderCopyType Enumeration | the copy types |
NodeReflectBuilderLabelType Enumeration | the label types |
Property Detail¶
CopyOption¶
-
NodeReflectBuilder.
CopyOption
¶ Returns or sets the copy option
-------------------------------------
Getter Method
Signature
CopyOption
Returns: Return type: NXOpen.CAE.NodeReflectBuilderCopyType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyOption
Parameters: copyOption ( NXOpen.CAE.NodeReflectBuilderCopyType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Increment¶
-
NodeReflectBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment
Parameters: increment (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
NodeReflectBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LabelOption¶
-
NodeReflectBuilder.
LabelOption
¶ Returns or sets the label option
-------------------------------------
Getter Method
Signature
LabelOption
Returns: Return type: NXOpen.CAE.NodeReflectBuilderLabelType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelOption
Parameters: labelOption ( NXOpen.CAE.NodeReflectBuilderLabelType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
NodeReflectBuilder.
Node
¶ Returns the node
-------------------------------------
Getter Method
Signature
Node
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX5.0.0.
License requirements: None.
Offset¶
-
NodeReflectBuilder.
Offset
¶ Returns or sets the offset
-------------------------------------
Getter Method
Signature
Offset
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset
Parameters: offset (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Plane¶
-
NodeReflectBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
NodeReflectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.