NodeReflectBuilderCopyType Enumeration

NXOpen.CAE.NodeReflectBuilder.CopyType is an alias for NXOpen.CAE.NodeReflectBuilderCopyType

class NXOpen.CAE.NodeReflectBuilderCopyType

Bases: object

the copy types

Enum Members

Enum Member Enum Member Description
ReflectOnly Reflect only
CopyReflect copy Reflect
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.