NodeProjectBuilder Class¶
-
class
NXOpen.CAE.
NodeProjectBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodeProjectBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodeProjectBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CopyOption | Returns or sets the copy option |
Geometry | Returns the geometry on which projection will happen |
Increment | Returns or sets the increment |
Label | Returns or sets the label |
LabelOption | Returns or sets the label option |
MethodOption | Returns or sets the method option |
Nodes | Returns the selected nodes to be extruded |
Offset | Returns or sets the offset |
PercentOffset | Returns or sets the percent offset |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the projection tolerance |
Vector | Returns or sets the vector along which projection will happen |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NodeProjectBuilderLabelType Enumeration | Option to use label/increment or offset |
NodeProjectBuilderNodeProjectTypes Enumeration | Represents the node project types |
NodeProjectBuilderProjectionMethodType Enumeration | Represents Projection Method |
Property Detail¶
CopyOption¶
-
NodeProjectBuilder.
CopyOption
¶ Returns or sets the copy option
-------------------------------------
Getter Method
Signature
CopyOption
Returns: Return type: NXOpen.CAE.NodeProjectBuilderNodeProjectTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyOption
Parameters: methodOption ( NXOpen.CAE.NodeProjectBuilderNodeProjectTypes
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Geometry¶
-
NodeProjectBuilder.
Geometry
¶ Returns the geometry on which projection will happen
-------------------------------------
Getter Method
Signature
Geometry
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX8.5.0.
License requirements: None.
Increment¶
-
NodeProjectBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment
Parameters: increment (int) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
NodeProjectBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LabelOption¶
-
NodeProjectBuilder.
LabelOption
¶ Returns or sets the label option
-------------------------------------
Getter Method
Signature
LabelOption
Returns: Return type: NXOpen.CAE.NodeProjectBuilderLabelType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelOption
Parameters: labelOption ( NXOpen.CAE.NodeProjectBuilderLabelType
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MethodOption¶
-
NodeProjectBuilder.
MethodOption
¶ Returns or sets the method option
-------------------------------------
Getter Method
Signature
MethodOption
Returns: Return type: NXOpen.CAE.NodeProjectBuilderProjectionMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodOption
Parameters: methodOption ( NXOpen.CAE.NodeProjectBuilderProjectionMethodType
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Nodes¶
-
NodeProjectBuilder.
Nodes
¶ Returns the selected nodes to be extruded
-------------------------------------
Getter Method
Signature
Nodes
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX8.5.0.
License requirements: None.
Offset¶
-
NodeProjectBuilder.
Offset
¶ Returns or sets the offset
-------------------------------------
Getter Method
Signature
Offset
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset
Parameters: offset (int) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PercentOffset¶
-
NodeProjectBuilder.
PercentOffset
¶ Returns or sets the percent offset
-------------------------------------
Getter Method
Signature
PercentOffset
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PercentOffset
Parameters: percentOffset (float) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Tolerance¶
-
NodeProjectBuilder.
Tolerance
¶ Returns or sets the projection tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tol (float) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Vector¶
-
NodeProjectBuilder.
Vector
¶ Returns or sets the vector along which projection will happen
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
NodeProjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.