NodeProjectBuilderNodeProjectTypes Enumeration

NXOpen.CAE.NodeProjectBuilder.NodeProjectTypes is an alias for NXOpen.CAE.NodeProjectBuilderNodeProjectTypes

class NXOpen.CAE.NodeProjectBuilderNodeProjectTypes

Bases: object

Represents the node project types

Enum Members

Enum Member Enum Member Description
ProjectOnly project only
CopyAndProject copy and project
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.