TestResult Class¶
-
class
NXOpen.CAE.ModelCheck.
TestResult
¶ Bases:
NXOpen.TransientObject
Represents quality checking result of a quality test
To obtain an instance of this class use CAE.ModelCheck.ElementTestResult.GetTestResults
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
TestType | Returns the test type |
TestValue | Returns the test value. |
ValidatedTestResult | Returns the validation result of comparing test value with the criteria value. |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
HasTestValue | Tells whether there is a test value associated with this test |
Property Detail¶
TestType¶
-
TestResult.
TestType
¶ Returns the test type
-------------------------------------
Getter Method
Signature
TestType
Returns: Return type: NXOpen.CAE.ModelCheck.TestValueTypesTestType
New in version NX8.5.0.
License requirements: None.
TestValue¶
-
TestResult.
TestValue
¶ Returns the test value.
An exception will be thrown f there is no test value associated with this test
-------------------------------------
Getter Method
Signature
TestValue
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
ValidatedTestResult¶
-
TestResult.
ValidatedTestResult
¶ Returns the validation result of comparing test value with the criteria value.
if no test value is associated this test, the result just indicates the test is passed or failed
-------------------------------------
Getter Method
Signature
ValidatedTestResult
Returns: Return type: NXOpen.CAE.ModelCheck.TestValueTypesResult
New in version NX8.5.0.
License requirements: None.