TestValueTypesTestType Enumeration¶
NXOpen.CAE.ModelCheck.TestValueTypes.TestType is an alias for NXOpen.CAE.ModelCheck.TestValueTypesTestType
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesTestType
¶ Bases:
object
the test types
Enum Members
Enum Member Enum Member Description JacobianZero JacobianRatio JacobianSign Volume AxisymmetricY When elements are modeled in XZ plane, check consistent Y. When elements are modeled in XY plane, check consistent Z. AxisymmetricX When elements are modeled in XZ plane, check X >= 0.0. When elements are modeled in XY plane, check Y >= 0.0. AspectRatio SkewAngle InteriorAngleMinimum InteriorAngleMaximum Taper WarpFactor FaceWarpCoefficient EdgePointLengthRatio EdgePointIncludedAngle LengthRatioOffset ParallelDeviation ShapeFactor Twist LengthMinimum LengthMaximum TetCollapse WarpageAngle CohesiveElement LaminateTaperRatio Ratio of longest edge to shortest edge in stacking direction for the elements that reference PCOMPS entries only. LaminateThicknessRatio Ratio of the difference between thickness in stacking direction as defined by grids and thickness as defined by ply thickness specification to the thickness in the stacking direction as defined by grids for the elements that reference PCOMPS entries only. Area -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-