ElementQualityCheckResultsTestSummary_Struct Struct¶
NXOpen.CAE.ModelCheck.ElementQualityCheckResults.TestSummary is an alias for NXOpen.CAE.ModelCheck.ElementQualityCheckResultsTestSummary_Struct
-
class
NXOpen.CAE.ModelCheck.
ElementQualityCheckResultsTestSummary_Struct
¶ Bases:
object
Reprents the summary data of a specified quality checking test type .
Constructor: NXOpen.CAE.ModelCheck.ElementQualityCheckResults.TestSummary()
Fields¶
Field | Description |
---|---|
TestType | the test type |
WorstTestValue | the worst test value of the specified test within all checked elements. |
HasTestValue | indicates whether the test has a test value. |
TestCount | indicates the total number of elements tested for this test |
ErrorCount | the count of elements with error results |
WarnedCount | the count of elements with warning results. |
TestType¶
-
ElementQualityCheckResultsTestSummary_Struct.
TestType
¶ the test type
-------------------------------------
Field Value Type:
NXOpen.CAE.ModelCheck.TestValueTypesTestType
WorstTestValue¶
-
ElementQualityCheckResultsTestSummary_Struct.
WorstTestValue
¶ the worst test value of the specified test within all checked elements.
which is only availabe for the test has a test value
-------------------------------------
Field Value Type:float
HasTestValue¶
-
ElementQualityCheckResultsTestSummary_Struct.
HasTestValue
¶ indicates whether the test has a test value.
If false, there is no test value associcated with this test
-------------------------------------
Field Value Type:bool
TestCount¶
-
ElementQualityCheckResultsTestSummary_Struct.
TestCount
¶ indicates the total number of elements tested for this test
-------------------------------------
Field Value Type:int