ElementQualityCheckResults Class¶
-
class
NXOpen.CAE.ModelCheck.
ElementQualityCheckResults
¶ Bases:
NXOpen.TransientObject
Represents the element quality checking result of
NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder
To obtain an instance of this class use CAE.ModelCheck.ElementQualityCheckBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ElementTestCount | Returns the total number of element tested during a test session |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetElementTestResultByIndex | Returns test results of each element |
GetTestSummary | Returns summary data of tests executed by NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder |
Structs¶
ElementQualityCheckResultsTestSummary_Struct Struct | Reprents the summary data of a specified quality checking test type |
Property Detail¶
Method Detail¶
Dispose¶
-
ElementQualityCheckResults.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
GetElementTestResultByIndex¶
-
ElementQualityCheckResults.
GetElementTestResultByIndex
¶ Returns test results of each element
Signature
GetElementTestResultByIndex(index)
Parameters: index (int) – Returns: Return type: NXOpen.CAE.ModelCheck.ElementTestResult
New in version NX8.5.0.
License requirements: None.
GetTestSummary¶
-
ElementQualityCheckResults.
GetTestSummary
¶ Returns summary data of tests executed by
NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder
Signature
GetTestSummary()
Returns: Return type: list of NXOpen.CAE.ModelCheck.ElementQualityCheckResultsTestSummary_Struct
New in version NX8.5.0.
License requirements: None.