ModeSetBuilder Class¶
-
class
NXOpen.CAE.
ModeSetBuilder
¶ Bases:
NXOpen.CAE.AlternateFemRepresentationSourceBuilder
Represents a
NXOpen.CAE.ModeSetBuilder
which can be used to create ModeSets.Not support KF.
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitAlternateFemRepresentationSource | Commits the changes that have been applied to the builder and returns the edited or newly created NXOpen.CAE.AlternateFemRepresentationSource |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableModesets | Get the mode sets available in the source file of the NXOpen.CAE.ModeSet |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SelectModeset | Select the mode set that should be used. |
SetFilePath | Sets the file path |
SetLengthUnit | Sets the length unit |
SetMassUnit | Sets the mass unit |
SetMeshCreationMode | Sets the mesh creation mode |
SetModesCanBeRenumbered | Allow the modes to be renumbered in case there are modes with the same index in the modeset |
SetName | Sets the name of the FemDataSet |
SetResultReference | Sets the result reference |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetAvailableModesets¶
-
ModeSetBuilder.
GetAvailableModesets
¶ Get the mode sets available in the source file of the
NXOpen.CAE.ModeSet
Signature
GetAvailableModesets()
Returns: The available mode set names. Return type: list of str New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SelectModeset¶
-
ModeSetBuilder.
SelectModeset
¶ Select the mode set that should be used.
The name should be one retrieved from
CAE.ModeSetBuilder.GetAvailableModesets()
. Should be called ifCAE.ModeSetBuilder.GetAvailableModesets()
returns several mode sets. This method is mandatory. If this method is not called, the mode set name corresponding to the empty string will be selectedSignature
SelectModeset(modeSetName)
Parameters: modeSetName (str) – The mode set name. New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetModesCanBeRenumbered¶
-
ModeSetBuilder.
SetModesCanBeRenumbered
¶ Allow the modes to be renumbered in case there are modes with the same index in the modeset
Signature
SetModesCanBeRenumbered(allowRenumbering)
Parameters: allowRenumbering (bool) – Allow renumbering flag. New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
ModeSetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.