AlternateFemRepresentationSourceBuilder Class¶
-
class
NXOpen.CAE.
AlternateFemRepresentationSourceBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.AlternateFemRepresentationSourceBuilder
which can be used to create FemDataSets.Not support KF.
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitAlternateFemRepresentationSource | Commits the changes that have been applied to the builder and returns the edited or newly created NXOpen.CAE.AlternateFemRepresentationSource |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFilePath | Sets the file path |
SetLengthUnit | Sets the length unit |
SetMassUnit | Sets the mass unit |
SetMeshCreationMode | Sets the mesh creation mode |
SetName | Sets the name of the FemDataSet |
SetResultReference | Sets the result reference |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CommitAlternateFemRepresentationSource¶
-
AlternateFemRepresentationSourceBuilder.
CommitAlternateFemRepresentationSource
¶ Commits the changes that have been applied to the builder and returns the edited or newly created
NXOpen.CAE.AlternateFemRepresentationSource
Signature
CommitAlternateFemRepresentationSource()
Returns: The object being edited, or the new object. Return type: NXOpen.CAE.AlternateFemRepresentationSource
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetFilePath¶
-
AlternateFemRepresentationSourceBuilder.
SetFilePath
¶ Sets the file path
Signature
SetFilePath(filepath)
Parameters: filepath (str) – Name of the file associated to the Fem Data Set. New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLengthUnit¶
-
AlternateFemRepresentationSourceBuilder.
SetLengthUnit
¶ Sets the length unit
Signature
SetLengthUnit(lengthUnit)
Parameters: lengthUnit ( NXOpen.Unit
) – Length unit used to read the data file.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetMassUnit¶
-
AlternateFemRepresentationSourceBuilder.
SetMassUnit
¶ Sets the mass unit
Signature
SetMassUnit(massUnit)
Parameters: massUnit ( NXOpen.Unit
) – Mass unit used to read the data file.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetMeshCreationMode¶
-
AlternateFemRepresentationSourceBuilder.
SetMeshCreationMode
¶ Sets the mesh creation mode
Signature
SetMeshCreationMode(creationMode)
Parameters: creationMode ( NXOpen.CAE.AlternateFemRepresentationSourceCreateMeshMode
) – Mesh creation mode used to read the data file.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
AlternateFemRepresentationSourceBuilder.
SetName
¶ Sets the name of the FemDataSet
Signature
SetName(name)
Parameters: name (str) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultReference¶
-
AlternateFemRepresentationSourceBuilder.
SetResultReference
¶ Sets the result reference
Signature
SetResultReference(pResultRef)
Parameters: pResultRef ( NXOpen.CAE.SimResultReference
) – Result Reference associated to the Fem Data Set.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
AlternateFemRepresentationSourceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.