MeshPointOnCurveBuilder Class¶
-
class
NXOpen.CAE.
MeshPointOnCurveBuilder
¶ Bases:
NXOpen.CAE.MeshPointBaseBuilder
Represents a
NXOpen.CAE.MeshPointOnCurveBuilder
To create a new instance of this class, use
NXOpen.CAE.MeshPointCollection.CreateMeshpointOnCurveBuilder()
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
Curve | Returns the node |
MeshPointToEdit | Returns or sets the base mesh point that will be replaced or edited after the commit operation (Edit Operation). |
NodeLabel | Returns or sets the node label assigned to mesh point so that node created on the mesh point will have that label. |
TParameter | Returns the t parameter |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Curve¶
-
MeshPointOnCurveBuilder.
Curve
¶ Returns the node
-------------------------------------
Getter Method
Signature
Curve
Returns: Return type: NXOpen.SelectIBaseCurveList
New in version NX5.0.2.
License requirements: None.
TParameter¶
-
MeshPointOnCurveBuilder.
TParameter
¶ Returns the t parameter
-------------------------------------
Getter Method
Signature
TParameter
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
Method Detail¶
Validate¶
-
MeshPointOnCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.