MechanicalLoadSumBuilder Class¶
-
class
NXOpen.CAE.
MechanicalLoadSumBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.MechanicalLoadSumBuilder
To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateMechanicalLoadSumBuilder()
New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
EvaluationFrequency | Returns the evaluation frequency |
EvaluationTime | Returns the evaluation time |
ReferenceCsys | Returns or sets the reference csys |
Tag | Returns the Tag for this object. |
UserSpecifiedUnit | Returns or sets the output result unit |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetLoads | The load objects |
GetObject | Returns the object currently being edited by this builder. |
GetSolution | The solution object |
GetSubcase | The subcase object |
SetLoads | Sets the loads |
SetSolution | The solution object |
SetSubcase | The subcase object |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MechanicalLoadSumBuilderUserUnit Enumeration | User Specified output unit |
Property Detail¶
EvaluationFrequency¶
-
MechanicalLoadSumBuilder.
EvaluationFrequency
¶ Returns the evaluation frequency
-------------------------------------
Getter Method
Signature
EvaluationFrequency
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
EvaluationTime¶
-
MechanicalLoadSumBuilder.
EvaluationTime
¶ Returns the evaluation time
-------------------------------------
Getter Method
Signature
EvaluationTime
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ReferenceCsys¶
-
MechanicalLoadSumBuilder.
ReferenceCsys
¶ Returns or sets the reference csys
-------------------------------------
Getter Method
Signature
ReferenceCsys
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCsys
Parameters: referenceCsys ( NXOpen.CoordinateSystem
) –New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
UserSpecifiedUnit¶
-
MechanicalLoadSumBuilder.
UserSpecifiedUnit
¶ Returns or sets the output result unit
-------------------------------------
Getter Method
Signature
UserSpecifiedUnit
Returns: Return type: NXOpen.CAE.MechanicalLoadSumBuilderUserUnit
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserSpecifiedUnit
Parameters: userSpecifiedUnit ( NXOpen.CAE.MechanicalLoadSumBuilderUserUnit
) –New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetLoads¶
-
MechanicalLoadSumBuilder.
GetLoads
¶ The load objects
Signature
GetLoads()
Returns: Return type: list of NXOpen.CAE.SimLoad
New in version NX5.0.1.
License requirements: None.
GetSolution¶
-
MechanicalLoadSumBuilder.
GetSolution
¶ The solution object
Signature
GetSolution()
Returns: Ask Solution Return type: NXOpen.CAE.SimSolution
New in version NX5.0.1.
License requirements: None.
GetSubcase¶
-
MechanicalLoadSumBuilder.
GetSubcase
¶ The subcase object
Signature
GetSubcase()
Returns: Ask Solutionstep Return type: NXOpen.CAE.SimSolutionStep
New in version NX5.0.1.
License requirements: None.
SetLoads¶
-
MechanicalLoadSumBuilder.
SetLoads
¶ Sets the loads
Signature
SetLoads(loads)
Parameters: loads (list of NXOpen.CAE.SimLoad
) – sets the loadsNew in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetSolution¶
-
MechanicalLoadSumBuilder.
SetSolution
¶ The solution object
Signature
SetSolution(solution)
Parameters: solution ( NXOpen.CAE.SimSolution
) – Set SolutionNew in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetSubcase¶
-
MechanicalLoadSumBuilder.
SetSubcase
¶ The subcase object
Signature
SetSubcase(subcase)
Parameters: subcase ( NXOpen.CAE.SimSolutionStep
) – Get SolutionstepNew in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
MechanicalLoadSumBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.