FemSignalProcessingApplication Class¶
-
class
NXOpen.CAE.
FemSignalProcessingApplication
¶ Bases:
NXOpen.Fields.IApplication
Implementation of the
NXOpen.Fields.IApplication
. This application provides support for attaching signal attributes (like acoustical weighting, energy/amplitude correction factors, …) on a field.Not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns the name of the application. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateSignalAttributes | Creates a new set of signal attributes that can be attached to a field. |
Method Detail¶
CreateSignalAttributes¶
-
FemSignalProcessingApplication.
CreateSignalAttributes
¶ Creates a new set of signal attributes that can be attached to a field.
The returned object is immutable, which means that all attributes are provided when creating the object. See
NXOpen.CAE.FemSignalProcessingSignalAttributes
for more informations about these attributes.Signature
CreateSignalAttributes(defaultVisualizationSpectrumScaling, defaultVisualizationCorrectionMode, amplitudeCorrectionFactor, energyCorrectionFactor, acousticalWeighting)
Parameters: - defaultVisualizationSpectrumScaling (
NXOpen.CAE.FemSignalProcessingSignalAttributesSpectrumScalings
) – - defaultVisualizationCorrectionMode (
NXOpen.CAE.FemSignalProcessingSignalAttributesCorrectionModes
) – - amplitudeCorrectionFactor (float) –
- energyCorrectionFactor (float) –
- acousticalWeighting (
NXOpen.CAE.FemSignalProcessingSignalAttributesAcousticalWeightings
) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
- defaultVisualizationSpectrumScaling (