IApplication Class¶
-
class
NXOpen.Fields.
IApplication
¶ Bases:
NXOpen.TaggedObject
Interface for all applications registered with the Field subsystem. Each application type should only be registered once with the Field subsystem. Each application class is identified by its name.
This is an abstract class, and cannot be created.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns the name of the application. |
Tag | Returns the Tag for this object. |