FacetProximityBuilder Class¶
-
class
NXOpen.CAE.
FacetProximityBuilder
¶ Bases:
NXOpen.Builder
Represents a
CAE.FacetProximityBuilder
builderTo create a new instance of this class, use
NXOpen.DebugSession.CreateFacetProximityBuilder()
Default values.
Property Value DisplayONOFFtoggle 1 DisplayOptionsEnum LinearFacets FacetCheckTolerance.Value 0.01 (millimeters part), 0.003937 (inches part) ListOptionsEnum Summary New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
DisplayONOFFtoggle | Returns or sets the display onofftoggle |
DisplayOptionsEnum | Returns or sets the display options enum |
FacetCheckTolerance | Returns the facet check tolerance |
ListOptionsEnum | Returns or sets the list options enum |
SelectGeometry | Returns the select geometry |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FacetProximityBuilderDisplayOptions Enumeration | List option for facet proximity to UG CAD : NX7. |
FacetProximityBuilderListOptionsType Enumeration | List option for facet proximity to UG CAD : NX7. |
Property Detail¶
DisplayONOFFtoggle¶
-
FacetProximityBuilder.
DisplayONOFFtoggle
¶ Returns or sets the display onofftoggle
-------------------------------------
Getter Method
Signature
DisplayONOFFtoggle
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayONOFFtoggle
Parameters: displayONOFFtoggle (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DisplayOptionsEnum¶
-
FacetProximityBuilder.
DisplayOptionsEnum
¶ Returns or sets the display options enum
-------------------------------------
Getter Method
Signature
DisplayOptionsEnum
Returns: Return type: NXOpen.CAE.FacetProximityBuilderDisplayOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayOptionsEnum
Parameters: displayOptionsEnum ( NXOpen.CAE.FacetProximityBuilderDisplayOptions
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FacetCheckTolerance¶
-
FacetProximityBuilder.
FacetCheckTolerance
¶ Returns the facet check tolerance
-------------------------------------
Getter Method
Signature
FacetCheckTolerance
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ListOptionsEnum¶
-
FacetProximityBuilder.
ListOptionsEnum
¶ Returns or sets the list options enum
-------------------------------------
Getter Method
Signature
ListOptionsEnum
Returns: Return type: NXOpen.CAE.FacetProximityBuilderListOptionsType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ListOptionsEnum
Parameters: listOptionsEnum ( NXOpen.CAE.FacetProximityBuilderListOptionsType
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectGeometry¶
-
FacetProximityBuilder.
SelectGeometry
¶ Returns the select geometry
-------------------------------------
Getter Method
Signature
SelectGeometry
Returns: Return type: NXOpen.CAE.SelectCAEBodyList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
FacetProximityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.