FacetProximityBuilderListOptionsType Enumeration¶
NXOpen.CAE.FacetProximityBuilder.ListOptionsType is an alias for NXOpen.CAE.FacetProximityBuilderListOptionsType
-
class
NXOpen.CAE.
FacetProximityBuilderListOptionsType
¶ Bases:
object
List option for facet proximity to UG CAD : NX7.5 onwards
Enum Members
Enum Member Enum Member Description Summary FullList -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-