ElementRotateBuilder Class¶
-
class
NXOpen.CAE.
ElementRotateBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementRotateBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementRotateBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the theta angle for translation in a cylindrical/spherical coordinate system |
Axis | Returns or sets the axis. |
CopyOption | Returns or sets the copy option . |
DistanceCopyOption | Returns or sets the distance option |
ElementDimension | Returns or sets the dimension of the elements to be rotated |
ElementSelection | Returns the selected elements |
ElementType | Returns the element type builder. |
Increment | Returns or sets the increment in label for each new element |
Label | Returns or sets the start label for the new elements |
LabelOption | Returns or sets the option to specify the start label and increment for the new elements OR specify an offset from the existing element labels |
MeshCollectorName | Returns or sets the name of the mesh collector which will hold the new elements |
MeshName | Returns or sets the name of the mesh that will hold the new elements |
NeutralName | Returns or sets the neutral name of the elements to be created |
NewMeshOption | Returns or sets the option to create a new mesh or add the new elements to an existing mesh |
NumCopy | Returns or sets the number of copies to be created for each selected element |
Offset | Returns or sets the offset to be used to generate new element labels |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementRotateBuilderCopyType Enumeration | the copy types |
ElementRotateBuilderDistanceType Enumeration | Distance - specify whether the translation distance is per copy or total |
ElementRotateBuilderElemDimensionType Enumeration | Dimension of the elements to be created |
ElementRotateBuilderLabelType Enumeration | Option to use label/increment or offset |
ElementRotateBuilderMethodType Enumeration | Translation method |
ElementRotateBuilderNewMeshType Enumeration | Option to create a new mesh or add the new elements to an existing mesh |
Property Detail¶
Angle¶
-
ElementRotateBuilder.
Angle
¶ Returns the theta angle for translation in a cylindrical/spherical coordinate system
-------------------------------------
Getter Method
Signature
Angle
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
Axis¶
-
ElementRotateBuilder.
Axis
¶ Returns or sets the axis.
-------------------------------------
Getter Method
Signature
Axis
Returns: Return type: NXOpen.Axis
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis
Parameters: axis ( NXOpen.Axis
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CopyOption¶
-
ElementRotateBuilder.
CopyOption
¶ Returns or sets the copy option .
-------------------------------------
Getter Method
Signature
CopyOption
Returns: Return type: NXOpen.CAE.ElementRotateBuilderCopyType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyOption
Parameters: inCopyoption ( NXOpen.CAE.ElementRotateBuilderCopyType
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DistanceCopyOption¶
-
ElementRotateBuilder.
DistanceCopyOption
¶ Returns or sets the distance option
-------------------------------------
Getter Method
Signature
DistanceCopyOption
Returns: Return type: NXOpen.CAE.ElementRotateBuilderDistanceType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceCopyOption
Parameters: distanceOption ( NXOpen.CAE.ElementRotateBuilderDistanceType
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementDimension¶
-
ElementRotateBuilder.
ElementDimension
¶ Returns or sets the dimension of the elements to be rotated
-------------------------------------
Getter Method
Signature
ElementDimension
Returns: Return type: NXOpen.CAE.ElementRotateBuilderElemDimensionType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElementDimension
Parameters: elementDimension ( NXOpen.CAE.ElementRotateBuilderElemDimensionType
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementSelection¶
-
ElementRotateBuilder.
ElementSelection
¶ Returns the selected elements
-------------------------------------
Getter Method
Signature
ElementSelection
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX12.0.0.
License requirements: None.
ElementType¶
-
ElementRotateBuilder.
ElementType
¶ Returns the element type builder.
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Increment¶
-
ElementRotateBuilder.
Increment
¶ Returns or sets the increment in label for each new element
-------------------------------------
Getter Method
Signature
Increment
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment
Parameters: increment (int) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
ElementRotateBuilder.
Label
¶ Returns or sets the start label for the new elements
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LabelOption¶
-
ElementRotateBuilder.
LabelOption
¶ Returns or sets the option to specify the start label and increment for the new elements OR specify an offset from the existing element labels
-------------------------------------
Getter Method
Signature
LabelOption
Returns: Return type: NXOpen.CAE.ElementRotateBuilderLabelType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelOption
Parameters: labelOption ( NXOpen.CAE.ElementRotateBuilderLabelType
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshCollectorName¶
-
ElementRotateBuilder.
MeshCollectorName
¶ Returns or sets the name of the mesh collector which will hold the new elements
-------------------------------------
Getter Method
Signature
MeshCollectorName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshCollectorName
Parameters: meshCollectorName (str) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshName¶
-
ElementRotateBuilder.
MeshName
¶ Returns or sets the name of the mesh that will hold the new elements
-------------------------------------
Getter Method
Signature
MeshName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshName
Parameters: meshName (str) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NeutralName¶
-
ElementRotateBuilder.
NeutralName
¶ Returns or sets the neutral name of the elements to be created
-------------------------------------
Getter Method
Signature
NeutralName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NeutralName
Parameters: neutralName (str) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewMeshOption¶
-
ElementRotateBuilder.
NewMeshOption
¶ Returns or sets the option to create a new mesh or add the new elements to an existing mesh
-------------------------------------
Getter Method
Signature
NewMeshOption
Returns: Return type: NXOpen.CAE.ElementRotateBuilderNewMeshType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewMeshOption
Parameters: newMeshOption ( NXOpen.CAE.ElementRotateBuilderNewMeshType
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumCopy¶
-
ElementRotateBuilder.
NumCopy
¶ Returns or sets the number of copies to be created for each selected element
-------------------------------------
Getter Method
Signature
NumCopy
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumCopy
Parameters: numCopy (int) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Offset¶
-
ElementRotateBuilder.
Offset
¶ Returns or sets the offset to be used to generate new element labels
-------------------------------------
Getter Method
Signature
Offset
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset
Parameters: offset (int) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
ElementRotateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.