ElementRotateBuilderDistanceType Enumeration¶
NXOpen.CAE.ElementRotateBuilder.DistanceType is an alias for NXOpen.CAE.ElementRotateBuilderDistanceType
-
class
NXOpen.CAE.
ElementRotateBuilderDistanceType
¶ Bases:
object
Distance - specify whether the translation distance is per copy or total
Enum Members
Enum Member Enum Member Description PerCopy distance specified is for each copy Total distance specified is total translation distance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-