DurabilityStrengthCollection Class

class NXOpen.CAE.DurabilityStrengthCollection

Bases: object

Represents a collection of event strength settings.

To obtain an instance of this class, refer to NXOpen.CAE.DurabilityManager

New in version NX8.5.0.

Methods

Method Description
CloneStrength Clones a durability event strength settings.
CreateEventstrengthsettingsBuilder Creates the builder object of durability event strength settings.
DeleteStrength Delete a durability event strength settings.
FindObject Finds an event strength settings with a specified name.

Method Detail

CloneStrength

DurabilityStrengthCollection.CloneStrength

Clones a durability event strength settings.

Signature CloneStrength(source)

Parameters:source (NXOpen.CAE.DurabilityStrength) – Source event strength settingss
Returns:Cloned event strength settingss
Return type:NXOpen.CAE.DurabilityStrength

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

CreateEventstrengthsettingsBuilder

DurabilityStrengthCollection.CreateEventstrengthsettingsBuilder

Creates the builder object of durability event strength settings.

Signature CreateEventstrengthsettingsBuilder(eventstrengthsettings)

Parameters:eventstrengthsettings (NXOpen.CAE.DurabilityStrength) –
Returns:
Return type:NXOpen.CAE.DurabilityEventStrengthSettingsBuilder

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

DeleteStrength

DurabilityStrengthCollection.DeleteStrength

Delete a durability event strength settings.

Signature DeleteStrength(eventstrengthsettings)

Parameters:eventstrengthsettings (NXOpen.CAE.DurabilityStrength) – The durability event strength settings to be deleted

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

FindObject

DurabilityStrengthCollection.FindObject

Finds an event strength settings with a specified name.

Signature FindObject(name)

Parameters:name (str) – name of the durability event strength settings
Returns:The durability event strength settings
Return type:NXOpen.CAE.DurabilityStrength

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)