DurabilityEventStrengthSettingsBuilder Class¶
-
class
NXOpen.CAE.
DurabilityEventStrengthSettingsBuilder
¶ Bases:
NXOpen.Builder
Represents a builder class for the event strength settings.
The event strength settings are the data which describe how to evaluate the strength and what to output for strength results.
To create a new instance of this class, use
NXOpen.CAE.DurabilityStrengthCollection.CreateEventstrengthsettingsBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
FactorOfSafety | Returns or sets the factor of safety. |
MarginOfSafety | Returns or sets the margin of safety. |
Name | Returns or sets the name. |
OrthotropicFailureCriterion | Returns or sets the orthotropic failure criterion. |
PerformOrthotropicAnalysis | Returns or sets the perform orthotropic analysis. |
StrengthSafetyFactor | Returns or sets the strength safety factor. |
StressCriterion | Returns or sets the stress criterion. |
StressType | Returns or sets the stress type. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DurabilityEventStrengthSettingsBuilderOrthotropicFailureCriterionEnum Enumeration | the orthotropic Failure criterion enum. |
DurabilityEventStrengthSettingsBuilderStressCriterionEnum Enumeration | the stress criterion enum. |
DurabilityEventStrengthSettingsBuilderStressTypeEnum Enumeration | the stress type enum. |
Property Detail¶
FactorOfSafety¶
-
DurabilityEventStrengthSettingsBuilder.
FactorOfSafety
¶ Returns or sets the factor of safety.
-------------------------------------
Getter Method
Signature
FactorOfSafety
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FactorOfSafety
Parameters: factorOfSafety (float) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MarginOfSafety¶
-
DurabilityEventStrengthSettingsBuilder.
MarginOfSafety
¶ Returns or sets the margin of safety.
-------------------------------------
Getter Method
Signature
MarginOfSafety
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MarginOfSafety
Parameters: marginOfSafety (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Name¶
-
DurabilityEventStrengthSettingsBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: title (str) – New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
OrthotropicFailureCriterion¶
-
DurabilityEventStrengthSettingsBuilder.
OrthotropicFailureCriterion
¶ Returns or sets the orthotropic failure criterion.
-------------------------------------
Getter Method
Signature
OrthotropicFailureCriterion
Returns: Return type: NXOpen.CAE.DurabilityEventStrengthSettingsBuilderOrthotropicFailureCriterionEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrthotropicFailureCriterion
Parameters: orthotropicFailureCriterion ( NXOpen.CAE.DurabilityEventStrengthSettingsBuilderOrthotropicFailureCriterionEnum
) –New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
PerformOrthotropicAnalysis¶
-
DurabilityEventStrengthSettingsBuilder.
PerformOrthotropicAnalysis
¶ Returns or sets the perform orthotropic analysis.
-------------------------------------
Getter Method
Signature
PerformOrthotropicAnalysis
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PerformOrthotropicAnalysis
Parameters: performOrthotropicAnalysis (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StrengthSafetyFactor¶
-
DurabilityEventStrengthSettingsBuilder.
StrengthSafetyFactor
¶ Returns or sets the strength safety factor.
-------------------------------------
Getter Method
Signature
StrengthSafetyFactor
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StrengthSafetyFactor
Parameters: strengthSafetyFactor (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StressCriterion¶
-
DurabilityEventStrengthSettingsBuilder.
StressCriterion
¶ Returns or sets the stress criterion.
-------------------------------------
Getter Method
Signature
StressCriterion
Returns: Return type: NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressCriterionEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StressCriterion
Parameters: stressCriterion ( NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressCriterionEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StressType¶
-
DurabilityEventStrengthSettingsBuilder.
StressType
¶ Returns or sets the stress type.
-------------------------------------
Getter Method
Signature
StressType
Returns: Return type: NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressTypeEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StressType
Parameters: stressType ( NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressTypeEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
Validate¶
-
DurabilityEventStrengthSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.