DataSourceCollection Class¶
-
class
NXOpen.CAE.
DataSourceCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.DataSource
.To obtain an instance of this class, refer to
NXOpen.CAE.PostScenarioManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateDataSourceBuilder | Creates a NXOpen.CAE.DataSourceBuilder that will be used to create a data source |
DeleteDataSource | Deletes a NXOpen.CAE.DataSource |
EditDataSourceBuilder | Creates a NXOpen.CAE.DataSourceBuilder that will be used to edit a data source |
FindObject | Finds a NXOpen.CAE.DataSource with the specified name. |
Refresh | Refreshes any cache held by Application Specific Post Processing with regards to the managed Data Sources. |
Method Detail¶
CreateDataSourceBuilder¶
-
DataSourceCollection.
CreateDataSourceBuilder
¶ Creates a
NXOpen.CAE.DataSourceBuilder
that will be used to create a data sourceSignature
CreateDataSourceBuilder()
Returns: Return type: NXOpen.CAE.DataSourceBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteDataSource¶
-
DataSourceCollection.
DeleteDataSource
¶ Deletes a
NXOpen.CAE.DataSource
Signature
DeleteDataSource(source)
Parameters: source ( NXOpen.CAE.DataSource
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
EditDataSourceBuilder¶
-
DataSourceCollection.
EditDataSourceBuilder
¶ Creates a
NXOpen.CAE.DataSourceBuilder
that will be used to edit a data sourceSignature
EditDataSourceBuilder(source)
Parameters: source ( NXOpen.CAE.DataSource
) –Returns: Return type: NXOpen.CAE.DataSourceBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
DataSourceCollection.
FindObject
¶ Finds a
NXOpen.CAE.DataSource
with the specified name.Signature
FindObject(name)
Parameters: name (str) – name of the layout state Returns: Return type: NXOpen.CAE.DataSource
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Refresh¶
-
DataSourceCollection.
Refresh
¶ Refreshes any cache held by Application Specific Post Processing with regards to the managed Data Sources.
Application Specific Post Processing caches some information about the referenced Data Sources for performance reasons, and under specific circumstances (e.g. modifying data sources outside the Pre/Post environment), this cached information might no longer be up to date. This method purges this information cache.
Signature
Refresh()
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)