DataSourceBuilder Class¶
-
class
NXOpen.CAE.
DataSourceBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.DataSourceBuilder
which can be used to create scenario data sources.No KF support.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
SourceFile | Returns or sets the selected input file |
SourceName | Returns or sets the data source name |
SourceObject | Returns or sets the selected source object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SourceFile¶
-
DataSourceBuilder.
SourceFile
¶ Returns or sets the selected input file
-------------------------------------
Getter Method
Signature
SourceFile
Returns: Return type: str New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
SourceFile
Parameters: filename (str) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SourceName¶
-
DataSourceBuilder.
SourceName
¶ Returns or sets the data source name
-------------------------------------
Getter Method
Signature
SourceName
Returns: source name Return type: str New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
SourceName
Parameters: sourceName (str) – source name New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SourceObject¶
-
DataSourceBuilder.
SourceObject
¶ Returns or sets the selected source object
-------------------------------------
Getter Method
Signature
SourceObject
Returns: Return type: NXOpen.CAE.IPostScenarioDataSource
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
SourceObject
Parameters: sourceObject ( NXOpen.CAE.IPostScenarioDataSource
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
Validate¶
-
DataSourceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.