DataProcessingBlockCollection Class¶
-
class
NXOpen.CAE.
DataProcessingBlockCollection
¶ Bases:
object
Represents a collection of DPM events.
To obtain an instance of this class, refer to
NXOpen.CAE.DataProcessing
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateBuilder | Creates the builder object of the DPM Block. |
DeleteBlock | Delete a durability event. |
FindObject | Finds a block with a specified name. |
Method Detail¶
CreateBuilder¶
-
DataProcessingBlockCollection.
CreateBuilder
¶ Creates the builder object of the DPM Block.
Signature
CreateBuilder(propertyName, dataTag)
Parameters: - propertyName (str) –
- dataTag (
NXOpen.NXObject
) –
Returns: Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteBlock¶
-
DataProcessingBlockCollection.
DeleteBlock
¶ Delete a durability event.
Signature
DeleteBlock(blockTag)
Parameters: blockTag ( NXOpen.CAE.DataProcessingBlock
) – The block to be deletedNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
DataProcessingBlockCollection.
FindObject
¶ Finds a block with a specified name.
Signature
FindObject(name)
Parameters: name (str) – name of the block Returns: The data processing block Return type: NXOpen.CAE.DataProcessingBlock
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)