CylinderBoundingVolume Class¶
-
class
NXOpen.CAE.
CylinderBoundingVolume
¶ Bases:
NXOpen.CAE.BoundingVolumePrimitive
Represents Box Bounding Volume for Selection Recipe
This is a sub object
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Containment | Returns or sets the contaiment for the Bounding Volume Primitive. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetCreationMethod | Gets the type for the Bounding Volume Primitive. |
GetCsysDiameterHeight | Gets the coordinate system, diameter and height for the Cylinder Bounding Volume. |
GetEndpointsDiameter | Gets the end points and diameter for the Cylinder Bounding Volume. |
SetCsysDiameterHeight | Sets the coordinate system, diameter and height for the Cylinder Bounding Volume. |
SetEndpointsDiameter | Sets the end points and diameter for the Cylinder Bounding Volume. |
Method Detail¶
GetCsysDiameterHeight¶
-
CylinderBoundingVolume.
GetCsysDiameterHeight
¶ Gets the coordinate system, diameter and height for the Cylinder Bounding Volume.
Signature
GetCsysDiameterHeight()
Returns: a tuple Return type: A tuple consisting of (centerCsys, diameter, cylinderHeight). centerCsys is a NXOpen.CoordinateSystem
. diameter is aNXOpen.Expression
. cylinderHeight is aNXOpen.Expression
.New in version NX12.0.0.
License requirements: None.
GetEndpointsDiameter¶
-
CylinderBoundingVolume.
GetEndpointsDiameter
¶ Gets the end points and diameter for the Cylinder Bounding Volume.
Signature
GetEndpointsDiameter()
Returns: a tuple Return type: A tuple consisting of (baseCenter, topCenter, diameter). baseCenter is a NXOpen.Point
. topCenter is aNXOpen.Point
. diameter is aNXOpen.Expression
.New in version NX12.0.0.
License requirements: None.
SetCsysDiameterHeight¶
-
CylinderBoundingVolume.
SetCsysDiameterHeight
¶ Sets the coordinate system, diameter and height for the Cylinder Bounding Volume.
Signature
SetCsysDiameterHeight(centerCsys, diameter, cylinderHeight)
Parameters: - centerCsys (
NXOpen.CoordinateSystem
) – - diameter (
NXOpen.Expression
) – - cylinderHeight (
NXOpen.Expression
) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- centerCsys (
SetEndpointsDiameter¶
-
CylinderBoundingVolume.
SetEndpointsDiameter
¶ Sets the end points and diameter for the Cylinder Bounding Volume.
Signature
SetEndpointsDiameter(baseCenter, topCenter, diameter)
Parameters: - baseCenter (
NXOpen.Point
) – - topCenter (
NXOpen.Point
) – - diameter (
NXOpen.Expression
) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- baseCenter (