ConstraintResolutionBuilder Class¶
-
class
NXOpen.CAE.
ConstraintResolutionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ConstraintResolutionBuilder
builder which can resolve conflicts between the two input constraints by a specified ruleTo create a new instance of this class, use
NXOpen.CAE.SimSolution.CreateConstraintResolutionBuilder()
New in version NX8.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.ConflictResolutionBuilder
instead.
Properties¶
Property | Description |
---|---|
PropertyTable | Returns the new Constraint’s property table which can be used to update its property |
ResolveRule | Returns or sets the resolution rule which will be used to resolve the conflict between the two input constraints |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConstraintResolutionBuilderRule Enumeration | Constraint Resolution Rule |
Property Detail¶
PropertyTable¶
-
ConstraintResolutionBuilder.
PropertyTable
¶ Returns the new Constraint’s property table which can be used to update its property
-------------------------------------
Getter Method
Signature
PropertyTable
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX8.0.0.
License requirements: None.
ResolveRule¶
-
ConstraintResolutionBuilder.
ResolveRule
¶ Returns or sets the resolution rule which will be used to resolve the conflict between the two input constraints
-------------------------------------
Getter Method
Signature
ResolveRule
Returns: Return type: NXOpen.CAE.ConstraintResolutionBuilderRule
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResolveRule
Parameters: resolutionRule ( NXOpen.CAE.ConstraintResolutionBuilderRule
) –New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
ConstraintResolutionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.