ConstraintResolutionBuilderRule Enumeration¶
NXOpen.CAE.ConstraintResolutionBuilder.Rule is an alias for NXOpen.CAE.ConstraintResolutionBuilderRule
-
class
NXOpen.CAE.
ConstraintResolutionBuilderRule
¶ Bases:
object
Constraint Resolution Rule
Enum Members
Enum Member Enum Member Description ApplyFirstConstraint apply first constraint on the intersection ApplySecondConstraint apply second constraint on the intersection AverageDofValues average dof values on the intersection AddDofValues add dof values on the intersection SpecifyDofValues specify dof values on the intersection IgnoreConflict specify dof values on the intersection -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-