SelectionRecipeLocation Class¶
-
class
NXOpen.CAE.Connections.
SelectionRecipeLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
SelectionRecipe | Returns or sets the Selection Recipe used for creating the location. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetXyzCoordinates | Gets the coordinates from the specified location. |
Property Detail¶
SelectionRecipe¶
-
SelectionRecipeLocation.
SelectionRecipe
¶ Returns or sets the Selection Recipe used for creating the location.
If the location type is not a Selection Recipe, this method will raise an error.
-------------------------------------
Getter Method
Signature
SelectionRecipe
Returns: Return type: NXOpen.CAE.SelectionRecipe
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionRecipe
Parameters: selectionRecipe ( NXOpen.CAE.SelectionRecipe
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)