FeEdgesLocation Class¶
-
class
NXOpen.CAE.Connections.
FeEdgesLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
GetFeEdges | Retrieve location edges. |
GetXyzCoordinates | Gets the coordinates from the specified location. |
SetFeEdges | Add location edges. |
Method Detail¶
GetFeEdges¶
-
FeEdgesLocation.
GetFeEdges
¶ Retrieve location edges.
Signature
GetFeEdges()
Returns: Edges used for location Return type: list of NXOpen.CAE.FEElemEdge
New in version NX12.0.0.
License requirements: None.
SetFeEdges¶
-
FeEdgesLocation.
SetFeEdges
¶ Add location edges.
Signature
SetFeEdges(edges)
Parameters: edges (list of NXOpen.CAE.FEElemEdge
) – Edges used for locationNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)