BoxBoundingVolume Class¶
-
class
NXOpen.CAE.
BoxBoundingVolume
¶ Bases:
NXOpen.CAE.BoundingVolumePrimitive
Represents Box Bounding Volume for Selection Recipe
This is a sub object
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Containment | Returns or sets the contaiment for the Bounding Volume Primitive. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetCreationMethod | Gets the type for the Bounding Volume Primitive. |
GetCsysEdgelengths | Gets the coordinate system and edge lengths for the Box Bounding Volume. |
GetDiagonalPoints | Gets the diagonal points for the Box Bounding Volume. |
SetCsysEdgelengths | Sets the coordinate system and edge lengths for the Box Bounding Volume. |
SetDiagonalPoints | Sets the diagonal points for the Box Bounding Volume. |
Method Detail¶
GetCsysEdgelengths¶
-
BoxBoundingVolume.
GetCsysEdgelengths
¶ Gets the coordinate system and edge lengths for the Box Bounding Volume.
Signature
GetCsysEdgelengths()
Returns: a tuple Return type: A tuple consisting of (centerCsys, length, width, height). centerCsys is a NXOpen.CoordinateSystem
. length is aNXOpen.Expression
. width is aNXOpen.Expression
. height is aNXOpen.Expression
.New in version NX12.0.0.
License requirements: None.
GetDiagonalPoints¶
-
BoxBoundingVolume.
GetDiagonalPoints
¶ Gets the diagonal points for the Box Bounding Volume.
Signature
GetDiagonalPoints()
Returns: a tuple Return type: A tuple consisting of (firstPoint, secondPoint). firstPoint is a NXOpen.Point
. secondPoint is aNXOpen.Point
.New in version NX12.0.0.
License requirements: None.
SetCsysEdgelengths¶
-
BoxBoundingVolume.
SetCsysEdgelengths
¶ Sets the coordinate system and edge lengths for the Box Bounding Volume.
Signature
SetCsysEdgelengths(centerCsys, length, width, height)
Parameters: - centerCsys (
NXOpen.CoordinateSystem
) – - length (
NXOpen.Expression
) – - width (
NXOpen.Expression
) – - height (
NXOpen.Expression
) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- centerCsys (
SetDiagonalPoints¶
-
BoxBoundingVolume.
SetDiagonalPoints
¶ Sets the diagonal points for the Box Bounding Volume.
Signature
SetDiagonalPoints(firstPoint, secondPoint)
Parameters: - firstPoint (
NXOpen.Point
) – - secondPoint (
NXOpen.Point
) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- firstPoint (