AutomaticMorphBuilder Class¶
-
class
NXOpen.CAE.
AutomaticMorphBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.AutomaticMorphBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateAutomaticMorphBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AssociationTolerance | Returns the option to tune geomtery association tolerance. |
OrphanNodeMovementOption | Returns or sets the option which indicates whether nodes in topologically modified region will be stationary, or move by adjacent nodes movement. |
SelectMesh | Returns the selected meshes |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AutomaticMorphBuilderOrphanNodeMovementType Enumeration | Orphan Node Movement Method - specify how the nodes move in topologically modified region. |
Property Detail¶
AssociationTolerance¶
-
AutomaticMorphBuilder.
AssociationTolerance
¶ Returns the option to tune geomtery association tolerance.
A node is associated to modified topo geometry, if the node is within specified tolerance.
-------------------------------------
Getter Method
Signature
AssociationTolerance
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OrphanNodeMovementOption¶
-
AutomaticMorphBuilder.
OrphanNodeMovementOption
¶ Returns or sets the option which indicates whether nodes in topologically modified region will be stationary, or move by adjacent nodes movement.
-------------------------------------
Getter Method
Signature
OrphanNodeMovementOption
Returns: Return type: int New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OrphanNodeMovementOption
Parameters: orphanNodeMovementOption (int) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectMesh¶
-
AutomaticMorphBuilder.
SelectMesh
¶ Returns the selected meshes
-------------------------------------
Getter Method
Signature
SelectMesh
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
AutomaticMorphBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.