AutomaticMorphBuilderOrphanNodeMovementType Enumeration¶
NXOpen.CAE.AutomaticMorphBuilder.OrphanNodeMovementType is an alias for NXOpen.CAE.AutomaticMorphBuilderOrphanNodeMovementType
-
class
NXOpen.CAE.
AutomaticMorphBuilderOrphanNodeMovementType
¶ Bases:
object
Orphan Node Movement Method - specify how the nodes move in topologically modified region.
Enum Members
Enum Member Enum Member Description BasedOnNbrMovement Based on adjacent nodes movement. Stationary Stationary in topologically modified region. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-