OnestepUnformCollection Class

class NXOpen.BodyDes.OnestepUnformCollection

Bases: object

Represents a collection of OnestepUnform

To obtain an instance of this class, refer to NXOpen.Part

New in version NX5.0.0.

Methods

Method Description
CreateOnestepBuilder Creates an Onestep Unform builder.

Method Detail

CreateOnestepBuilder

OnestepUnformCollection.CreateOnestepBuilder

Creates an Onestep Unform builder.

Signature CreateOnestepBuilder(onestepunform)

Parameters:onestepunform (NXOpen.Features.Feature) – Features.Feature to be edited
Returns:OnestepUnformBuilder object object
Return type:NXOpen.BodyDes.OnestepUnformBuilder

New in version NX6.0.0.

License requirements: nx_onestep_analysis (“NX Onestep Analysis”) OR nx_general_packaging (“NX General Packaging”) OR die_engineering (“DIE ENGINEERING”) OR aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)