DesignElementBuilderPositioningOption Enumeration¶
NXOpen.Assemblies.DesignElementBuilder.PositioningOption is an alias for NXOpen.Assemblies.DesignElementBuilderPositioningOption
-
class
NXOpen.Assemblies.
DesignElementBuilderPositioningOption
¶ Bases:
object
Represents the positioning option of a design element.
Enum Members
Enum Member Enum Member Description AbsoluteOrigin Applies absolute origin position on the design elements Maintain Maintains the existing positions of the design elements. Applicable only if the edit action type is set to DesignElementBuilderEditActionType.Category
AsSpecified Applies the specified position on the design elements -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-