DesignElementBuilderEditActionType Enumeration

NXOpen.Assemblies.DesignElementBuilder.EditActionType is an alias for NXOpen.Assemblies.DesignElementBuilderEditActionType

class NXOpen.Assemblies.DesignElementBuilderEditActionType

Bases: object

Represents the edit action on a design element

Enum Members

Enum Member Enum Member Description
Category
Partitions
Effectivity
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.